Article
NEC requirement
The language in Article 215 in Section 215.15 (Barriers) is very similar to the language that was created for Section 230.62 (Service Equipment Barriers). Similar hazards exist in both of these locations.
These requirements recognize the increased “risk” for equipment fed directly from transformers and tap conductors. Barriers are required for panelboards, switchboards, switchgear, or motor control centers supplied by feeder taps in 240.21(B) or transformer secondary conductors in 240.21(C).
When the disconnecting device, to which the tap conductors are terminated, is in the OPEN position, you cannot have any exposed energized parts.
NEC 2023 code change/intention
Rationale for change
What are the 2023 NEC updates pertaining to barriers?