Download document () of 20

Water use

Water stewardship

As global demand for water grows, we continue to reduce our water consumption and implement responsible water practices. Our processes are not particularly water intensive, but water is critical to many of our operations. And as water stress becomes more pronounced in some areas in which we operate, this will continue to be an area of focus for us.
Since 2015 we’ve reduced our water consumption by more than 710,000 cubic meters
710k
Since 2015 we’ve reduced our water consumption by more than 710,000 cubic meters
In 2019 we reduced our water consumption 14% from our 2015 baseline
14
%
In 2019 we reduced our water consumption 14% from our 2015 baseline
The amount of water we have saved since 2015 would fill more than 284 Olympic swimming pools
284
The amount of water we have saved since 2015 would fill more than 284 Olympic swimming pools

Measuring and reporting on progress

We set annual water reduction goals, and to meet them, we focus on our largest water users and areas of high water stress. On an annual basis, we evaluate our water use management practices, measure our results and report across our facilities. In 2019, we reduced water consumption by 7% compared to the prior year.