Download document () of 20

Business Continuity | Eaton | toy force

Toy Force_Q3_Summer_banner_no text.jpg
BIGS will help you respond to the unique challenges that you may be facing when supporting your customers to maintain their business continuity wherever they are.
BIGS Mission is to keep businesses safe with reliable power management & monitoring. He’s proud to support your customers with the resources they need to strengthen the security across their business.

Help your customers manage power with:

Energy-saving power protection for workstations.

The Eaton Ellipse ECO is a slim-line power protection device with a built-in, high-performance surge-protection enabling energy savings of up to 25% compared to previous-generation UPSs.
Ellipse_Eco_DC.jpg

High-quality protection against power surges and dips – and in the event of a power failure, the Eaton 3S UPS also acts as an emergency power supply.

The perfect choice to secure internet modems, televisions, PCs, game consoles and network equipment.

3s-ups-din-fm2.jpg
Eaton Protection Box is a best in class multi outlet surge protection device for critical equipment in residential or professional environments. 
Eaton Protection BOX

Ready for Success?

Eaton Protection Strip is an affordable multi-outlet surge protection device for sensitive equipment in residential or professional environments.
Eaton Protection Strip