Date: March 27, 2018
- Eaton’s new Power Xpert XGIS technology can dramatically reduce annual maintenance requirements by upwards of 40 percent
- Enhances safety through sealed high-voltage components and reduced maintenance requirements
- Can reduce switchgear footprint requirements by nearly 70 percent compared to air-insulated technology in some voltage classes
PITTSBURGH, PA — Power management company Eaton today announced new gas-insulated switchgear designed to provide powerful advantages in safety and reliability for critical power applications in data centers, oil and gas, mining, process industries, and other commercial and industrial applications. With the majority of high-voltage components in a sealed compartment, Eaton’s new
Power Xpert XGIS technology is designed to reduce maintenance requirements, reduce the need for operators to interface with the equipment and substantially reduce space requirements in some voltage classes.
Utilizing sealed tank design, Eaton’s Power Xpert XGIS switchgear is virtually maintenance free and can help reduce the potential for arc faults – contributing to dramatic enhancements in reliability and safety. Maintenance requirements for any equipment inside sealed tank are eliminated. Additionally, the possibility of animal intrusion and the likelihood of incidental contact are reduced by the equipment’s design.
“When it comes to electrical power distribution equipment, Eaton is a long-time industry leader with a trusted portfolio of medium-voltage solutions. Today, we’re able to offer both air and gas-insulated technologies for global applications,” said Jeremy Novotney, product line manager at Eaton. “Eaton’s Power Xpert XGIS is built to perform and last for decades, while reducing overall ownership costs through minimal maintenance and enhancing safety through robust arc protection – enabling customers to maximize space for revenue-generating equipment.”
Eaton’s gas-insulated switchgear enables energized parts to be closer together, which can significantly reduce space requirements, especially in 27 and 38 kilo-voltage classes. The equipment can be applied in both new construction and retrofit applications where floor space is limited.
Eaton’s Power Xpert XGIS can be applied in indoor applications, including both electrical rooms and integrated power assemblies or e-houses. It is third-party tested and certified to International Electrotechnical Commisssion (IEC) 62271-200.
Eaton’s electrical business is a global leader with expertise in power distribution and circuit protection; backup power protection; control and automation; lighting and security; structural solutions and wiring devices; solutions for harsh and hazardous environments; and engineering services. Eaton is positioned through its global solutions to answer today’s most critical electrical power management challenges.
Eaton is a power management company with 2017 sales of $20.4 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 96,000 employees and sells products to customers in more than 175 countries. For more information, visit
Eaton.com.
Contact
Ann Marie Halal, (440) 523-4418
Regina Parundik, (412) 559-1614