Date: September 13, 2017
PITTSBURGH, PA — Power management company Eaton today announced a contract to provide the circuit protection for a 12-megawatt solar project in Nicaragua. Eaton circuit breakers will be used to help enhance the safety and reliability of the large-scale photovoltaic system using string inverters rated for 1,500 volts (V) direct current (DC).
Eaton is providing its molded case circuit breakers to New Jersey based Olson Motor and Control Company, which is designing and fabricating the alternating current (AC) collection panels for the project. The installation is expected to be complete in the second quarter of 2018.
“Adding to Nicaragua’s growing renewable energy portfolio, the project will help the country continue to reduce its historical dependence on imported fuel to generate power and enhance electrical power reliability,” said John Vernacchia, Americas segment manager for renewable energy at Eaton. “Eaton is a long-time leader in circuit protection solutions with an expansive portfolio of both circuit breakers and fuses that will help enhance the safety and reliability of the installation.”
Under the contract with Olson Motor and Control Company, Eaton will supply its NMZ series molded case circuit breakers, rated for the 800V AC output from the solar inverters used in the project. The output voltage was established by the string inverter manufacturer, and the circuit breakers used are rated up to 1000V DC.
The circuit protection used in the project is listed to the International Electrotechnical Commission (IEC) 60204 standard for main switching and IEC 60947 for isolation. With a robust portfolio of electrical balance of system solutions for solar installations, and a team of experienced engineers, Eaton provides power management equipment and software tailored to customer requirements and the skills needed to successfully complete a project, from initial design and application assistance through post-installation measurement, verification and maintenance. For more information, visit www.eaton.com/solar.
Eaton’s electrical business is a global leader with expertise in power distribution and circuit protection; backup power protection; control and automation; lighting and security; structural solutions and wiring devices; solutions for harsh and hazardous environments; and engineering services. Eaton is positioned through its global solutions to answer today’s most critical electrical power management challenges.
Eaton is a power management company with 2016 sales of $19.7 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 95,000 employees and sells products to customers in more than 175 countries. For more information, visit Eaton.com.
Contact US
Ann Marie Halal, (440) 523-4418
Regina Parundik, (412) 559-1614