Date: March 6, 2017
TINTON FALLS, N.J. … The Filtration Division of power management company Eaton will demonstrate how its filtration solutions designed for hydraulic and lubrication oil applications bring a breath of fresh air into process efficiency and reliability at HMI trade show in hall 21, booth B15, April 24 to 28 in Hannover, Germany.
The exhibition program includes high-performing filtration solutions to remove solids and water from hydraulic and lubrication fluids used in compressors, gearboxes, power units, lubrication modules, mobile hydraulics and factory equipment. Using any of these filtration solutions help keep fluid operating at peak efficiency, prevent contamination harming hydraulic systems, and minimize downtime and operation costs.
One highlight is Eaton’s Twinfil™ TWF 4000 filter unit especially redesigned for gear lubrication systems in wind turbines. Whether used onshore, offshore or in cold climates, it reliably filters and de-aerates oil under the most challenging operating conditions including cold starts for top system performance and uptime. The anodized aluminum body in a compact design is sea waterproof for maximum corrosion resistance and reduces weight by more than 75 percent compared to standard options in carbon steel or cast iron.
Eaton will also showcase a representative selection of its range of filter housings for stationary and mobile hydraulic systems that extend product life of the fluids with better fuel usage. The simplified mounting of the HPX manifold mounted pressure filters provides filtration directly at the point needed and prevents contaminants from passing downstream during element changes. The easy-to-change TEF 426 in-tank return line filter prevents contamination from entering the reservoir and reduce the possibility of oil spillage during element changes. The silica gel granules in the BFD tank breather filters absorb moisture to protect oil from oxidation.
Complementing the filter housing offering, Eaton shows a wide range of filter elements for trouble-free operation when filtering abrasive or water-based fluids and cooling lubricants. More than 4,000 high-performance filter elements are available with various filter materials, different construction types and micron ratings to help protect critical system components and achieve cleanliness class requirements.
The exhibition program will be rounded out by the CCS 4 contamination control system. This system helps to promptly initiate actions and cost-saving measures before any failure can occur. It enables users to evaluate the precise condition of the system fluid by knowing particle size distribution of contamination plus water saturation and fluid temperature.
Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit www.eaton.com/filtration.
Eaton is a power management company with 2016 sales of $19.7 billion. Eaton provides energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton has approximately 97,000 employees and sells products to customers in more than 175 countries. For more information, visit www.eaton.com.
Contact US
Margaret DeAngelis, (732) 212-4703