What are the primary benefits for network closet applications of switching to lithium-ion UPS batteries?
What lithium-ion network UPSs does Eaton offer?
Are there any wallmount lithium-ion UPSs?
Does Eaton offer any non-real sine wave UPSs with a lithium-ion battery?
Can I use a lithium-ion EBM with a VRLA 9PX UPS?
Are lithium-ion EBMs the same size as VRLA EBMs?
Can I attach extra batteries to the 5P and 9PX lithium-ion UPS models?
How many lithium-ion EBMs can I deploy with a rackmount lithium-ion 9PX UPS?
Where do I need to put the 9PX lithium-ion EBMs?
How many rackmount lithium-ion UPS can I install in a network closet?
What is the recommended operating temperature for a network closet with a lithium-ion UPS?
Do I need to leave extra space in the rack for airflow around a rackmount lithium-ion UPS?
What codes apply to rackmount lithium-ion UPSs?
Do you need an Eaton field technician to install a rackmount lithium-ion UPS?
No, there is no increased risk. An excerpt from an application note on lithium-ion battery safety explains "As part of DOT/UN38.3 testing, the case temperature of cells may not exceed 170°C (338°F). Since the LFP (Lithium iron phosphate) cells used in the 5P 1U lithium-ion UPS have a thermal runaway point much greater than this temperature, the risk of thermal runaway when exposed to situations like the test conditions is further reduced."
Read the full lithium-ion UPS battery safety application note here.
We have material safety data sheets (MSDS) and UL9540A test reports that show gasses are only released during a fire.
Download the MSDS for Samsung lithium-ion batteries.
Lithium battery management systems and battery monitoring systems, like Cellwatch and BTech, have the following similarities:
Lithium battery management systems differ from Cellwatch/BTECH, in the below capabilities:
What are the BTUh numbers when float charging lithium-ion UPS batteries?
See the Eaton customer drawings for BTUh levels. This heat is negligible, and does not typically affect HVAC calculations for the room.
Download the Samsung lithium-ion drawing here.
What are the BTUh levels during discharge of lithium-ion UPS batteries?
| Model | Weight | 
| Samsung 136 | 120 lbs | 
| Samsung 128 | 113 lbs | 
Can lithium batteries ship internal to the battery cabinet?
Yes, all vendors’ lithium-ion UPS battery cabinets communicate by Modbus TCP. The customer’s connection is via a TCP/IP (RJ45) connector from the main battery BMS module on the vendor’s cabinet/system.
NOTE: The Modbus TCP provides no alarm history. Information is real time, unless the user creates an external logging program.
Will Brightlayer eventually be connected to lithium-ion battery cabinets?
Why can we use 2x 3/0 cables with a 600A breaker in the Samsung cabinet? Seems too small?
Cable sizing for our batteries is not considered continuous operation, so we can use different ratings than standard permanent continuous operation tables per NEC. Consult the battery cabinet installation and operation manual, or the customer site plan drawing for allowable cable sizes.
We evaluated 2x 3/0 cables for use in our Samsung solution with UL, based on temperature rise test method. That’s where the recommendation comes from in our site plan. That’s how the product was evaluated by UL and hence the recommendations in our site plan.
The lithium cells in many of our lithium-ion battery units are composed of LFP (lithium iron phosphate). Each cell includes built-in over charge protection, pressure vent, anti-puncture ceramic coating, and a barrier on the positive LFP electrode to help mitigate short circuiting from any dendritic growth. Also, our BMS monitors and controls every cell within the battery pack to mitigate conditions which may encourage dendrite growth.
For more information on dendrites in lithium-ion batteries, read Eaton’s latest application note.
| Manufacturer | kWh capacity | Seismic zone | Power source | 
| Samsung | 32.6 kWh for 128S 34.6 kWh for 136s | Zone 4 and is OSHPD certified for UL9540A black cabinet | Samsung requires a 'UPS protected' source for the BMS. Gen 1 (white cabinet units), have a transformer in the conduit landing box that steps up to 208Vac from the UPS to 480Vac to run the cabinet from a 208 output UPS. Gen 2 UL9540A (black cabinet units) should be selected with a 1-phase 120/240V protected power source for use with a 208V UPS or a 480 V 3-phase source for a 480V or 600V UPS. In these Gen 2 systems, there is no transformer in the conduit landing box; the battery cabinet internal power supply will be provisioned with a 480Vac or 208Vac input based on the user's BMS voltage selection at the time of order. 
 | 
What vendors have we offered previously?
LG Chem cabinets populated with a single string or a double string of battery modules. LG Chem has discontinued this UPS battery, but many are deployed in the field, and will continue to be supported.
LiiON cabinets that have been installed in several locations. This manufacturer still offers this battery, but Eaton does not support its use on our products. Any service on these systems will be provided by LiiON.
The vendor warrants that when the battery is installed per vendor's instructions, operated within vendors environmental guidelines, and charged by the UPS as specified, the battery system will provide at least 78-80% of its initial capacity at the 10-year mark. If the battery or string fails to provide that capacity, it will be replaced at no charge. Labour is not covered, but a labour charge can be added to a battery system quote. The battery must be operated within the environmental specifications and cycle life limits set by the battery vendor. Data recordkeeping is the responsibility of the user (like VRLA). If the evidence indicates that the battery has been misused:
Can we supply copies of each vendor’s warranty document?
Can different vendor’s batteries be mixed?
Refer to the installation manual part # 164000729, shipped with each cabinet.
Conduit bushings or cable glands are required by code (NFPA 75 article 300.4(G) in the US and Canada, unless the room is restricted to authorized personnel only. Cable may not ‘waterfall’ into the cabinet from an overhead tray, for example, in a room or environment that is not restricted. Some inspectors have waived this requirement, but we will ship conduit landing kits with all standard lithium cabinets.
The Conduit landing assembly is mounted to the cabinet onsite. Instructions are provided. Total cabinet height would be an issue otherwise.
Download installation instructions for lithium-ion battery cabinets.
It is important to note that Eaton should not be the official source for these answers. Legal liabilities preclude our ability to act as the authority on any of this information. Clients are responsible for interpretation of and compliance to the appropriate local codes. However, we do want to provide general information on what clients should be aware of prior to the sale of lithium-ion battery systems. Both national and local codes could apply, and various codes may exceed or supersede our generic interpretations. Codes that may apply are, but not limited to:
The requirements and wording in all the above codes are similar but not identical. Different exceptions or exclusions could apply.
Room location: Not greater than 75’ above or 30’ below the lowest fire department access level unless successful UL9540A testing and FMEA analysis convinces AHJ to approve.
Seismic: a. Must comply with IBC Section 16, which describes the building structure, not the battery cabinet, but Samsung has been evaluated to seismic Zone 4 and is OSHPD certified with their latest (black) cabinets, when installed according to manufacturer’s instructions.
Ventilation: The below is not different than that which is required for VRLA installations.
What fire codes permit indoor installations of lithium-ion batteries?
To meet NFPA 855 requirements, does there need to be 3’ of spacing on the front and back, and both sides of the lithium-ion UPS battery cabinet?
Have you heard of any instances where an AHJ did not accept 9540A testing and required the increased 3’ spacing, per their criteria?
IFC 1206 and NFPA 855 are not retroactive, so installations that took place before they were enacted (in 2018 and 2019, respectively) do not need to comply. New battery installations or expansions of existing ones will need to comply.
To comply, a lithium-ion battery installation must meet these requirements:
Contact an AHJ inspector for any planned new additions.
What UL listings do our battery offerings carry?
For Samsung products:
UL 1642 for the batteries
UL 1973 for battery modules and systems
UL 1998 for the BMS (part of UL 1973 testing)
UL 9540A large scale fire testing; for Samsung black cabinets (Note: 9540A is a test method, not a ‘listing’ like UL9540). We have copies of the UL 9540A test report available on request for evaluation by the client or their AHJ.
What parts of the lithium-ion UPS battery installation is handled by the Eaton CSE vs. the electrical contractor?
Contractor places the empty cabinets, secures the battery cabinet to the floor of the building following the installation manual instructions, installs the conduit landing kit, runs wire and conduit for AC control power (480V or 208V 3W+G for Samsung) and installs and connects all power and control wiring between the battery cabinets and the UPS.
Eaton field engineers install the battery modules and other components in each cabinet for Samsung and connects the power and communication cabling internal to the cabinet. Eaton CSE performs the battery cabinet software setup and commissioning and makes applicable changes to the UPS charging functions, based on battery vendor’s set points.
Should DC cable lengths from each lithium battery cabinet to the UPS be identical?
With the absence of a standardised commissioning test for lithium batteries, we expect that commissioning would be somewhat similar to that of VRLA and should include the following: