Panelboards are used to safely distribute electricity throughout commercial and industrial facilities. A panelboard is a component of an electrical distribution system which divides an electrical power feed into branch circuits, while providing a protective circuit breaker or fuse for each circuit, in a common enclosure. A panelboard services to protect branch circuits from overloads and short circuits. Panelboards are designed to meet CSA C22.2 No. 29 and NEMA Standard PB1.
Switchboards and panelboards provide a similar functionality in a power distribution system. Panelboards are typically flush mounted or surface mounted and are limited to a maximum of 1,200 A incoming current (main). Switchboards are free-standing units that are front connected and, like panelboards, require only front access.
However, switchboards can allow for both front and rear access if desired. Switchboards can contain bussing and overcurrent devices up to 5,000 A. Where panelboards are designed to CSA C22.2 No. 29, switchboards are governed by UL 891.
Eaton offers general purpose panelboards for both circuit breaker (Pow-R-Line 1X, 2X, 3X) and fusible switch applications.
The choice of specific panelboard is dependent on:
Panelboards are constructed and typically dispatched as three separate primary components.
The five-sided enclosure itself, commonly called the ‘case’ or ‘box’ is typically made of galvanised steel and is either flush mounted or wall mounted.
Eaton’s EZ-trim incorporates a unique, one-piece design that allows the trim to be installed in seconds with no additional hardware or tools.
To match the construction process, the panelboard cases are typically dispatched first, followed by the interiors and the trims.
In addition to these primarily components, panelboards also include a label that provides information regarding the unit’s electrical ratings and manufacturing date, filler plates used to cover any unused spaces and a circuit directory card, located on the inside of the door.
The branch devices in a panelboard provide overcurrent protection for downstream devices. Most often both functions are provided by a moulded case circuit breaker. However, fusible switches can also be provided.
Eaton’s panelboards are built around Eaton’s Power Defense circuit breaker technology and Bussmann series fuse technology.
Panelboards can be supplied with electronic metering devices to monitor both incoming power to the panel as well as the power distributed through individual branch devices.
These meters can communicate via common industry protocols as part of an overall building energy management system. They can aid in complying with local energy codes or be part of your overall IoT/Industry 4.0 strategy.
Voltage spikes and surges can find their way into your facility from an outside disturbance or can manifest itself from equipment within your facility. Surge protection devices (SPDs) protect sensitive downstream electronic devices from the damaging effects of voltage surges or spikes.
Panelboard mounted SPDs can either be side-mounted or integrated design. Side-mounted units come pre-wired in a separate enclosure and are field-mounted and wired to the panel in the field.
Integrated surge protection devices, like Eaton’s SPD series, are factory mounted directly to the panelboard chassis. In addition to time and space savings, an integrated SPD increases system protection by reducing let-through voltage due to the zero-lead length design.
Find out about the many advantages of integrating surge protection inside power distribution equipment.
Panelboards, as well as other power distribution assemblies like switchboards and switchgear, carry a short-circuit current rating that defines the amount of fault current that the equipment is designed to withstand. There are three protection systems used to protect low voltage power distribution systems. They are:
Fully rated protection – where all overcurrent devices are rated for the full prospective short-circuit current at their line side terminals throughout the system. In a fully rated system, the short-circuit current rating of the panelboard is determined by the short-circuit current rating of the lowest rated overcurrent device in the panelboard
Selectively coordinated protection – A fully rated system where the overcurrent device closest to the fault will open first, thus isolating the faulty circuit.
Series rated protection – A short-circuit interrupting rating assigned to a combination of two or more overcurrent protective devices that are connected in series and in which the rating of the downstream device(s) in the combination is less than the series rating. Series ratings are also known in the industry as integrated ratings, series combination ratings and series connected ratings.
In a series rated system, the overcurrent devices in series in the protective scheme must have been tested and listed by Underwriters Laboratories (UL), for series combination use in the system.
Eaton’s currently published series ratings can be found in the current version of the panelboard and switchboard series rating information manual.