Need product support?
CYME user portal: my.cyme.com
P: 450 461 3655 or 800 361 3627 (Canada and USA)
Questions before you buy
Eaton’s CYME Load Relief DER Optimisation module equips engineers with a tool to efficiently design non-wire alternatives to mitigate capacity issues on critical grid assets.
An increasing number of utilities are being requested to systematically evaluate non-wire alternatives against traditional solutions when planning for significant capital expenditure which is essential to maintain and improve grid performance. While the engineering analyses standing behind traditional solutions have been mastered for several decades, the technical know-how required to optimally site and size utility-scale generation and energy storage systems generally remains a highly specialised expertise.
Eaton’s CYME Load Relief DER Optimisation module helps engineers with the evaluation of load relief projects using battery energy storage systems (BESS) as well as dispatchable and non-dispatchable generation. The module bundles two distinct algorithms, one for the optimisation of BESS and dispatchable generation and one for the sizing of non-dispatchable generation.
The dispatchable DER optimisation analysis optimally sites, sizes and sets the converter controls of BESS and dispatchable, electronically-coupled generators (ECG) with the objective of reducing the loading on strategic grid assets. Simulation results unfold in a variety of outputs, including summary and detailed reports as well as heat maps highlighting optimal sites for BESS and dispatchable ECG.
The non-dispatchable DER sizing analysis determines the required generator size to mitigate assets overloads. The analysis supports up to three different types of technology simultaneously (e.g. PV, wind energy conversion system, etc.) and handles each technology's specific behaviour. In terms of results, for each asset experiencing an overload over the simulation period, the analysis provides the required active power generation to mitigate user-defined levels of overload occurrences (e.g. 70%, 95% and 99% of overload occurrences).
The Load Relief DER Optimisation module turns weeks of engineering into minutes of computation and supports utilities in the modernisation of their planning framework, an unavoidable step towards the alignment of their practices with the climate and clean energy goals of the 21st century.
The primary objective of the analysis is to shave overloads at a user-defined device. Its simulation parameters include:
The primary objective of the analysis is to remove a user-defined amount of overload occurrences at each device of a network. Its simulation parameters include:
The BESS model is composed of many different components. The main part is the battery module that stores the active power and transfers it by charging or discharging the battery cells using internal DC/DC converters controlled by the battery management system. Power is then transferred to the AC side by the AC/DC converter. Using the capability of the converter, reactive power can be transferred in both directions, to and from the grid.
The amount of power that transits in both directions (charging/consuming and discharging/generating) is managed by the storage controller that determines, depending on its control settings and on network measurements, how much active and reactive power must be transferred to/from the network.
Several control types are supported, including power monitoring, DER monitoring and volt-var controls, to name a few.
Beyond optimal locations, sizes and converter settings, the simulation results unfold into a variety of intuitive outputs, including summary and drill-down reports, as well as heat maps highlighting the best sites for integrating BESS and dispatchable ECG.
The module can be used alone* or can harness the power of the Steady-State Analysis with Profiles module to automatically determine the maximum energy demand and time parameters of the overloaded device.
*The CYME distribution analysis base package (CYMDIST) is required.
Eaton’s CYME Load Relief DER Optimisation module equips engineers with a tool to efficiently design non-wire alternatives to mitigate capacity issues on critical grid assets.
Need product support?
CYME user portal: my.cyme.com
P: 450 461 3655 or 800 361 3627 (Canada and USA)
Questions before you buy